Part Number: UCC28740 Other Parts Discussed in Thread: TPS25740B , , PMP11451 , UCC28051 , PMP11455 Hi,
I am designing portable AC/DC converter with max 20V / 5A or 20V/3A typical.
I am planning to use a single design for two different applications.
1) Power…
Other Parts Discussed in Thread: TPS25740B , BQ25703A , BQ25703AEVM-732 , TPS65986EVM Hi All,
I am designing a Power bank which has Type-C PD (Power delivery) support.
So My charger requirement are as below,
2-3 Cell battery charger (14V 20000mA battery…
Hi Ikon,
If you are only interested in USB Power Delivery then the TPS25740B can perform that job without the need for serial flash chip config. The TPS25740B DFP PD controller that uses a resistive divider circuitry to implement the default voltage setting…
Hi Vivek,
Very sorry for the delay! At a high level, since this is an adapter application, I recommend using the TPS25740B since this is capable of your 20V rail. I recommend looking at the TPS23740BEVM-741 as it is 5A capable.
The EVM as an input voltage…
Part Number: TPS25740BEVM-741 Hi USB Team,
Good afternoon, my customer is interested in the Altium files for the TPS25740B EVM - I noticed these files aren't available in the tool folder, can you provide them over E2E?
Thank you!
Regards,
~John
Hi Zhifeng,
Since you don't need super speed lines and sbu lines, but need to handle PD negotiations, I would recommend the TPS25740B device. It's a type-C and USB PD source controller. The TPS65983B has more features than what your application is…
Hi Nguyen,
Looking through the datasheet, I do not think this part will work for a Type-C PD application. Yes, it will be able convert a 5V input into a 20V output. It will not be able to source the necessary current (5A) amount that is needed for PD…
Part Number: TPS25740A Other Parts Discussed in Thread: TPS25740B , TPS25741A Team,
My customer is working on a project using our TPS25740A, and has a few questions:
I’m testing with the TPS25740A, and I think I’m seeing a violation according to the datasheet…