Part Number: TPS25750 Hello,
I have got a couple of questions about the TPS25750 behavior:
1) I2Cm bus not working
At my setup it is not possible to access the I2Cm bus by the I2Cr and I2Cw commands. The TPS25750 responds correctly to the I2Cr…
Part Number: TPS25750 Tool/software: Hi expert,
My customer (CosMX) is looking for suitable devices which can support PD3.1 and QC protocol, do we have suitable devices? Thanks.
Best Regards,
Ryker
Part Number: TPS25751 Other Parts Discussed in Thread: TPS25750 , Tool/software: Hello,
We had a functional design with the TPS25750 internal switch variant. The design has been updated to swap in the TPS25751.
After the swap (new board spin,…
Part Number: TPS25751 Other Parts Discussed in Thread: TPS25750 , BQ25792 Tool/software: We are using the TPS + BQ25792 combination. After replacing the TPS25750 with the newer one, and download the new firwmware. We found that we can't set the bq25792…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25730 , BQ25798 Tool/software: Hi, I am a beginner in tps25750. i want it to control type-c to get 20V input. (now is 5V)
The TPS25750DRJKR ( without EEPROM) I2Cs is connected to MCU ( STM32L4A6VGTX…
Part Number: TPS25750 Dear TI,
I configured the limit input voltage as 15V - 3A and flashed it into eeprom.
But with some adapters, it was able to negotiated 15V, some didn't, it shows ~19V.
Attached is the adapter which provide 19V.
Any suggestion…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25751 Tool/software: The local schematic design is shown in the figure. When the charger is not connected, the TPS25750 can communicate successfully with the charger and set the charging voltage…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25751 Tool/software: Is it possible to configure GPIO1 of the TPS25750 as 'UFP_DFP_Event' and use it as the USB-ID signal, where DFP = 'High' operates in Host mode (P/D) and UFP = 'Low' operates…
Part Number: TPS25750 Other Parts Discussed in Thread: BQ25792 Tool/software: Hi,
I use the TPS25750 with the BQ25792 in a battery operated device.
The device is strapped for "always enable sink" in dead battery mode.
When the battery is discharging…