Part Number: TPS25751 Other Parts Discussed in Thread: TPS26750 Hi.
I want to check TPS25751 spec. please check it.
PD version : PD 3.2
max PDP : 100W
max PDO : 20V, 5A
PD 3.2 DPS (Dynamic Power supply) : support
External EEPROM : normally…
Part Number: TPS25751 Dear Sir,
I have a few technical questions regarding the configuration and programming of the TPS25751:
When selecting "Flash to Device" in the GUI tool, does this refer to burning the configuration file onto an external…
Part Number: TPS25751 Other Parts Discussed in Thread: TPS65987DDKEVM TPS25751 delivers only SOUCE function without battery
Select the resistance of the FB line of the DC-DC CONVERTER as the switch Power generation of 5V, 9V, 15V, 20V 3A specifications…
Part Number: TPS25751 Other Parts Discussed in Thread: USB-PD-CHG-EVM-01 , , TPS25750 Hello,
I have a USB-PD-CHG-EVM-01 and I'm following the instructions to configure the binary in the web tool. On the very first step where I need to select the TPS25751…
Part Number: TPS25751 Hi TI Team,
We are currently using the TPS25751 USB Type-C PD controller in our design and would like to clarify the mechanism for determining the USB data role (DFP/UFP) from the controller.
Context:
The TPS25751 is interfaced…
Part Number: TPS25751 Hi team,
My customer is evaluating the specifications of the TPS25751. I understand that the GPIO pins of the TPS25751 do not support behavior where the pin state changes automatically based on the Sink_PDO_ that the IC negotiates…
Part Number: TPS25751 Other Parts Discussed in Thread: USB-PD-CHG-EVM-01 , , Hi,
We are using the TPS25751 on the USB-PD-CHG-EVM-01 dev board. Using the USBCPD Application Customization Tool V1.1.1, we are trying to set GPIO5 to Open Drain Mode. We…
Part Number: TPS25751 Hi team,
My customer is considering adopting the TPS25751. They are evaluating it on the EVM as a Sink‑side application. They would like to configure two Sink PDOs: 5 V/3 A and 20 V/2 A. However, when a 15 V‑output adapter is connected…
Part Number: TPS25751 Other Parts Discussed in Thread: BQ25792EVM , I have copyied the BQ25792EVM module schemtic and I have paired it with a TPS25751 usb pd controller. I have a werid issue in which if i dont have a battery attached to the system it…
Part Number: TPS25751 Other Parts Discussed in Thread: TPS26750 , Hello TI Expert,
I am debugging the TPS25751 chip and referring to the document "Using an Embedded Controller (EC) to Load a Patch Bundle Directly to the TPS25751 or TPS26750". During…