Part Number: TPS25762-Q1 Hello. I have developed a circuit that incorporates the TPS25762-Q1 for USB-C charging and a Realtek RTL8152B-VB-CG network adapter for use with an iPad. Schematic below. Before configuring the TPS25762-Q1, I was able to get the…
Part Number: TPS25762-Q1 Hi,
I have a customer who uses the chip of TPS25762, and would like to know whether the firmware supporting 65W can be provided?
If the customer applies on the official website simultaneously, can we speed up the processing?…
Part Number: TPS25762-Q1 Hi support team,
is the EEPROM absolutely necessary or can it be left out?
I thought that if you can load the firmware via USB-C or via I2C (MCU), you could omit the EEPROM?
Please give me a clear statement.
Thank you
Part Number: TPS25762-Q1 HI
I have selected TPS25762 for USB PD 30W application, seems this chip will not support 24V or 32V input voltage ?, let me know any similar chip will support 24 V input or higher.
Seems TPS25762 maximum input voltage…
Part Number: TPS25762-Q1
Hi, Support Team
For PD controller, although the Vin Max of TPS25762CQRQLRQ1 is 40V but recommended Vin is only 18V. The Vin Max of our system would be 26V (OVP triggered point of VBAT), is it ok to use without any performance…
Part Number: TPS25762-Q1 Other Parts Discussed in Thread: TPS25772-Q1 , PMP40933 Hello, I have the following questions:
1.) Do you have any additional documents or a typical application circuit for the component as a pure USB-C power supply (charger)…
Part Number: TPS25762-Q1 Hi Team,
I would like to ask if there is an available Pspice model for TPS25762-Q1? or is there a similar device with an available Pspice model that can be used?
Thank you.
Regards,
Marv
Part Number: TPS25762-Q1 Other Parts Discussed in Thread: TPS254900A-Q1 Hi Team,
Could you kindly advise:
1) What's the behavior of TPS25762-Q1's PA_DP/PA_DM PIN after BC1.2 negotiation is done? Will these 2ports turn to Hi-Z internal?
2) Customer…
Part Number: TPS25762-Q1 Hi, Support Team
We have some question for bin file read/write to EEPROM
Q1:What’ the default status of GPIO0, input/output?
Q2:Plan to use TPS25762-Q1 GPIO0 for control the TVSP index selection between 0 to 5 ,Could GPIO0…