Part Number: TPS25762-Q1 Hi Team,
Is the GPIO0 setting disabled to a high impedance state?
Can getting date from I2C channel 2 ? (output voltage/current reading)
Thanks
Part Number: TPS25762-Q1 Hi,
As subject, could the device support input voltage 32V?
I saw DS shown 40V max on page one but I'm not sure any condition for this spec?
Part Number: TPS25762-Q1 Hi Expert:
Our customer is asking TPS25762CQRQLRQ1 material is halogen free or low halogen ? do we have the product material list could provide to customer?
thank you
Roy
Part Number: TPS25762Q1EVM Hi, Support Team
We reference TPS25762EVM and design target is to support 27W power for down device.
Q1: For calculation Vin power consumption is about 12V, 2.81A
Want to confirm is it ok to use 3x10uF 0603 & 2x0.1uF 0402 for…
Part Number: TPS25762-Q1 Hi Sir,
My customer is asking the TPS257xx-Q1 devices if have pass the the certification of UFCS(Universal Fast Charging Specification for Mobile Devices)?
New Universal Fast Charging Standard Announced in China: https://www.gizmochina…
Part Number: TPS25762-Q1 Hello, I'm looking through the datasheet and can't find any description how to read data from an MCU.
Can you provide information on what type of data can be obtained through telemetry and how to get it with the I2C2t…
Part Number: TPS25762-Q1 Burning firmware through portA will interrupt. The error screenshot is shown below. Is it a problem with the eeprom specification?
The current eeprom is not in the recommended list. The specific model is GT24C512.
Thanks
All…
Hi Damian, there are SPICE models for the TPS25762 controller but none specifically for the PMP40934. The spice model on the product page below might be a good start for your design.
https://www.ti.com/product/TPS25762-Q1#design-development
Looking at…
Hello L B,
The TPS25830-Q1 does not support PD as it is a Type-C and BC1.2 charge port converter with max output up to 5V and 3.5A.
Our automotive PD controller solutions are the TPS25762-Q1 (single-port) and TPS25772-Q1 (dual-port). Both devices supports…