The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: TPS25772-Q1 Tool/software: Hi team,
I want to confirm how to estimate thermal generation.
In case of Vin=13.5V, Vout/Iout=20V/3A, efficiency is around 96%.
Power loss is 60Wx4%=2.4W. Since ψJB=7.2C/W, deltaT=17.28C.
Seeing from test…
Part Number: TPS25772-Q1 Tool/software: HI team,
We designed the TPS25772-Q1 but it doesn't work.
1. VIN/VEN is correctly supplied to the device.
2. The device is outputting the correct LDOs voltage.(LDO_5V/3.3V/1.5V...OK)
3. The TVSP terminal is…
Part Number: TPS25772-Q1 Other Parts Discussed in Thread: TPS25772DQ1EVM , TPS25762-Q1 Tool/software: Hi, TI E2E teams
I have a project uses the chip of TPS25772-Q1.
I referred to the TPS25772DQ1EVM for the design.
Currently, I have confirmed that Ven…
Part Number: TPS25772-Q1 Tool/software: Dear TI experts,
Could you support measuring phase margin and gain margin of TPS25772-Q1 (buck boost module) on customer's PCB?
Best regards,
Chase
Part Number: TPS25772-Q1 Tool/software: Hi team,
Does its output power capability depend on which device is connected? We checked below.
All laptop and smartphone could be charged with 15W w/o issue.
Toshiba Lenova (X13) is charged as fast-charge; 30…
Part Number: TPS25772-Q1 Tool/software: Dear TI experts,
My customer considers TPS25772-Q1 for their new project. End product is wired charging module for car.
And they have a question about power sharing.
- Can TPS25772-Q1 set separate charging value…
Part Number: TPS25772-Q1 Tool/software: Hi Team,
TPS25772-Q1 can meet below condition?
Input: DC14V
When single output: A port: QC 36W C port: PD/QC 36W
When two OUTs are output at the same time: A port: QC 18W C port: PD/QC 27W
Part Number: TPS25772-Q1 Tool/software: Dears,
We want to use TPS25772-Q1 as a car USB charger for two type-C ports, if the two ports sharing 65W? Thank you~
Part Number: TPS25772-Q1 Other Parts Discussed in Thread: TPS257XX-Q1-GUI Tool/software: Hello Expert,
Could you please add description for each items on attached excel file?
PITS:TPS257xx Q1 GUI.xlsx
Our customer making FW using GUI but some parameter…
Part Number: TPS25772Q1EVM-CO-149 Tool/software: I have already purchased the TPS25772Q1EVM-CO-149 evaluation board and confirmed that the TPS257xx-Q1-GUI 1.4.0 is compatible with my development board. I am now planning to integrate the TPS25772-Q1 into…