Part Number: TPS25810 Hello,
Hello,
I am trying to add to my project a USB 3.0 type C port for connecting a mouse or keyboard to a host (NVIDIA Jetson Orin) . Could you please review and let me know if anything should be changed?
Part Number: TPS25810 Other Parts Discussed in Thread: HD3SS3220 , TUSB321 , Dear Team,
We provide Type-C Spec -> 5V/5A solution for customer as below,
Option 1:
HD3SS3220 -> CC Logic + MUX - https://www.ti.com/product/HD3SS3220
TPS259470 -> 5V/5A…
Part Number: TPS25810 hi,
Is there a power sequence to supply the TPS25810 itself? Is there no sequence for supplying voltage to the IN1 pin, IN2 pin, AUX pin, etc.? In other words, even if 5V is applied to the IN2 pin, is it OK if no voltage is applied…
There is no output pin from the TPS25810 that would trigger upon a plug event, which would be needed for switching on/off a FET connected to the IN pin of the TPS2546. This is why the TPS2546 is enabling the TPS25810.
I see no issues with your schematic…
Part Number: TPS25810
hi Teams:
Please help check the schematic diagram of TPS25810, and the requirements are as follows:
1.3A output
2. Can pass USB-C certification
3. The USB-C port only has power when the backend is connected to Device,
Part Number: TPS25810-Q1 Other Parts Discussed in Thread: HD3SS3212-Q1 , , TPD3S716-Q1 Hi
We need to implement USB type-C for automotive application, I survey the solution are HD3SS3212-Q1+ TPS25810-Q1, however, we need to perform all USB signals+VBUS with…
Hi Kevin,
The main difference from your schematic and our recommendation is on U6 and R19 on the OUT pins of the TPS25810. I would suggest trying to short across R19 to remove any resistance from the OUT pins of the TPS25810 and the VBUS pins of the USB…
Part Number: TPS25810 hi teams:
1.The general fast charging protocols for TYPE C include QC3/QC2/PD3.0/PD2.0. Which protocol does TPS25810 support for TYPE C fast charging?
2. What configuration does the interface circuit need to be matched with the mobile…