Part Number: TPS25830A-Q1 Other Parts Discussed in Thread: TPS25840-Q1 Hi TI Team, Please find the schematic of TPS25830A-Q1 - TPS25830AQCWRHBRQ1 CDC_USB2.0.pdf for review, Kindly share your valuable feedback on the same.
Project Details:
Segment…
Part Number: TPS25830A-Q1 Hi Team,
I am estimating the power dissipation of the TPS25830A-Q1 device for thermal simulation and would like to confirm whether my approach is correct.
PD = VIN × IIN × (1 – Efficiency) – 1.1 × IOUT^2 × DCR in Watt
…
Part Number: TPS25830A-Q1 Other Parts Discussed in Thread: TPS25831-Q1 , Hi,
I am designing a Type-C phone charger using the TPS25830A and I have a question.
I don't want to use the USB functionality. Do I need to connect the USB Data+/- pair to the…
Part Number: TPS25830A-Q1 Tool/software: Hi TI,
Can I use TPS25830A-Q1 to control CC1=Rd or CC2=Rd?
TPS25830A-Q1 Can only identify CC signals and report them?
Thanks
Part Number: TPS25830A-Q1 Hi team,
I would like to know if there is a TEST mode of TPS25830A-Q1, and is it possible to unexpectedly entrt this test mode during power-on, resulting in no output?
Regards,
Eileen
Part Number: TPS25830A-Q1 Tool/software: Hi TI team The following are our use cases with the TPS25830A, 1) Charging external devices over the USB connector, Android Auto and Apple car play. 2) Flashing and ADB - VBUS will be sourced from external devices…
Part Number: TPS25830A-Q1 Hi PI Team,
My customer is looking into a USB type C application for an IVI silver box, consumer side mounted to trim panel (no electronics at consumer connector) in which he's never worked on an application like this and neither…
Part Number: TPS25830A-Q1 Hi team,
I would like to know if there is a TEST mode of TPS25830A-Q1, and is it possible to unexpectedly entrt this test mode during power-on, resulting in no output?
Regards,
Eileen
Part Number: TPS25830A-Q1
Hi team
Based on the description of plug polarity detection, tps25830A-q1 only act as a DFP device, that means that tps25830A-Q1 acts as power source and SA8797 acts as data master when SA8797+TPS25830A-Q1 with type C connector…