Part Number: TPS25846-Q1 Hello Expert,
Could you please provide input imepdance of RT/SYNC pin?
Customer is using external SYNC operation so they worry that the negative impact from termination.
If you cannot provide detailed design value, rough…
Part Number: TPS25846-Q1 Tool/software: Hello, TI Team
I am testing the fault function of the TPS25846 on my board.
Q1:I want to trigger the fault signal by shorting the output terminal. However, the fault signal of the TPS25846 cannot be triggered…
Part Number: TPS25846-Q1 Tool/software: Hello, TI Team
I am testing TPS25846-q1 part on my board.
Q1:I want to trigger the fault signal by shorting the output terminal. However, the fault signal of the TPS25846 cannot be triggered. What is the reason…
Part Number: TPS25846-Q1 Other Parts Discussed in Thread: TPD4S480 Tool/software: Dear Experts,
Our product designed based on TPS25846-Q1 currently needs to pass the GB/T 28046.2 standard test. The short-circuit protection test requires all input and…
Part Number: TPS25846-Q1 Tool/software: Hi Team,
Does this IC automatically manage the handshaking with DP_IN & DM_IN pins or i need to use any other controller along with this? I didn't connect any resistors on these lines and DP_OUT & DM_OUT are left…
Part Number: TPS25846-Q1 Tool/software: Hello, could you provide us with the loop compensation Bode plots of the TPS25846Q1 chip under different scenarios (power part, feedback system, system open loop)?
Part Number: TPS25840-Q1 Other Parts Discussed in Thread: TPS25846-Q1 Tool/software: Hi team,
The customer is considering making the LM25830-Q1 and LM25846-Q1 schematics compatible. I found that there are some differences in the design. How should the…
Part Number: TPS25846-Q1 Tool/software: Dear Sirs,
1、Are there any differences in the USB eye diagram when testing in different modes below? Which mode should be chosen?We found that selecting Client Mode for testing failed and SDP mode for testing…
Part Number: TPS25846-Q1 Please help confirm the parameter EN/UVLO. I understand that the minimum requirement for lowering the voltage level is 0.3V; Its pull-up enable has a minimum of 1.14V and a maximum of VIN=36V (maximum withstand voltage