Part Number: TPS25846-Q1 When the load short circuit is eliminated, the TPS25846 will automatically restore to normal operation?
If yes, could you please clarify the algorithm?
Part Number: TPS25846-Q1 Hello Sir:
We have using TPS25846-Q1 on our new project.
We are not familiar this device.
Would you please help us to check the schematic and layout?
And if you have any EMC strategy on this circuit please also help to mention us…
Part Number: TPS25846-Q1 Hello Sir:
We are drawing TPS25846 schematic and we have below requirements.
1. output power from TPS25846 to device should be over 12W, and needs to support IOS device and Android device.
2. if the output connector cable length…
Part Number: TPS25846-Q1 Hi Expert,
Our customer use TPS25846-Q1. In datasheet, the output cap should be 3*22uF under 2.1MHz. But the customer put one 22uF near the output and put one 100uF cap a little far from 22uF. As you can see in below schematic…
Part Number: TPS25846-Q1 Hi team,
The customer uses MTB020N03KN3, but can only stand 1A. Could you please help them to find the reason?
Regards,
Cathy Cai
Part Number: TPS25846-Q1 We used the TPS25846 in our project between SOC and USB port. I want to do signal integrity for USB differential data with Hyperlynx. How can I get the IBIS modle of TPS25846 ?
Part Number: TPS25846-Q1 Other Parts Discussed in Thread: TPS25831-Q1 , TPS25833-Q1 Hi team,
According to BC1.2 , the maximum current in CDP mode is 1.5A. But the customer need 2.1A-2.4A current in CDP mode.
1) Could the device provide such large current…
Part Number: TPS25846-Q1 Hi Team,
Is that possible for the master controller to communicate through DP/DM to enable 2.1A/2.4A charging for TPS25846-Q1?
Regards,
Jie
Part Number: TPS25846-Q1 Hi team,
I would like to keep VBUS active up to 4.8A for 1ms.
Is that possible to set the current limit to minimum 4.8A?
regards,