Part Number: TPS25924 Other Parts Discussed in Thread: TPS2663 Hi Team,
We are planning to add e-fuse in with battery power pack of 16A1P size. Vbattery Pack = 58.4V and Ich =3A, Idisch = 18Amp.
Please suggesst the e-fuse or Hot-swap controller with…
Part Number: TPS25924 I am using a eFuse TPS259240 operating in the overcurrent in the linear region- what is the behavior expected?
eFuse TPS259240
Rlim=68.1k
2.7A is the Ilimit. I max is 2.3A. Please help answer the below questions.
a) For 500uS…
Part Number: TPS25924 Tool/software: Hi All,
I have a question about the BFET terminal of the TPS25924. What is the sink current of the BFET terminal?
Best Regards, Ishiwata
Part Number: TPS25924 Tool/software:
"The TPS259240 is burned out. Measurements show that PINs 3, 4, 5, 6, 7, and 8 are shorted to ground. Please help verify if there are any issues with the circuit design. There have already been more than ten cases…
Part Number: TPS25924 Tool/software: Hi TI experts,
We used TPS259241 for a hotswap design.
1. Startup behavior: the startup waveform looks different when i put passive probe on DVDT pin, once probe is added to DVDT cap, the VOUT ramping looks nonlinear…
Part Number: TPS25924
Hi All,
I have a question about TPS259241.
The capacitance of CINT is typically 70pF.
Please tell me the maximum and minimum values of CINT. Or, by what maximum percentage will the value change?
Best Regards, Ishiwat…
Part Number: TPS25924 Hi All,
I have a question regarding TPS259241. Is it okay to use an electrolytic capacitor for VOUT? Also, are there any regulations regarding the installation location of the output capacitor? Is the neighborhood good?
Best…
Part Number: TPS25924
Hi All,
I have a question about TPS259241.
TPS259241 is an Auto retry product, will the device shut down if there is a output short circuit? Or will it return automatically?
Best Regards, Ishiwata