Part Number: TPS25940 I am using the TPS25940L and I occasionally get UV Faults or Short Circuit faults when I extract the device it is monitoring. Instead of latching this fault (I have observed that all faults are latched) I would like to use the A…
Part Number: TPS25940 Hi TI support team,
I use TPS25940 as automotive application, due to the power dissipation of internal MOSFET, I change the dV/dT capacitor to 100pF.
I measure the slew rate of TPS25940, could you help me check the ramp time…
Part Number: TPS25940 Hi TI team,
I use TPS25940 at automotive application. When power input is 13V, it can not output power successfully, however it can not output power when I using near 15V/16V power input.
I found a Phenomenon that when I turn…
Part Number: TPS25940 Hi Team,
According to e2e post below, I can assume Tj=160(thermal sutdown threshold) and calculate the acceptable maximum power.
However, the absolute maxmum Tj in datasheet is 150 ºC , Tj beyond 150 ºC may cause permanent damage…
Part Number: TPS25940 We're looking for the max. power dissipation with package type. Could you share this for customer's thermal evaluation! Very thanks.
Regards
Brian W
Part Number: TPS25940-Q1 Dear team,
1. Can our device work normally when the load current is 100mA he 18mA respectively? If can, what are the current sampling accuracy? What is the resolution?
2. Can our device's IN pin withstand 18V for 1hour, 26…
Part Number: TPS25940 Other Parts Discussed in Thread: TPS25942L , Hi team,
My customer is using TPS25942L, and considering using TPS25940L to replace it.
This is same situation with https://e2e.ti.com/support/power-management-group/power-management…
Part Number: TPS25940 Other Parts Discussed in Thread: TPS25942L Hi team,
My customer is using TPS25942L, and considering using TPS25940L to replace it.
I see the only difference is DMODE of TPS25942L and DEVSLP of TPS25940L, but both these pins will…