Part Number: TPS25942A Other Parts Discussed in Thread: TPS25942EVM-635 Hello everyone,
I am considering using the TPS25942A in my design.
While reviewing the User’s Guide for the TPS25942EVM-635 (SLVUA56, June 2014), I noticed the following note…
Part Number: TPS25942A Other Parts Discussed in Thread: TPS25942EVM-635 Hi Team,
I have a question regarding the note in Section 4.5.4 Current Limit Tests on page 9 of the TPS25942EVM-635 User's Guide, which states:
"Measuring Current Limit values…
Part Number: TPS25942A Tool/software: TPS25942A-Power block diagram.pdf
Dear Arush and TI Team
Thank you for your support so far.
This is regarding Oring IC TPS25942A,
1. As I said earlier, these ICs are giving problems in my design. I bypassed…
Part Number: TPS25942A Other Parts Discussed in Thread: TPS2420 , , TPS2660 , TPS25947 , TPS2597
Tool/software:
Hi team, Our customer needs TPS25942A and TPS2420, TPS2660 IEC62368 Ed.3. They seems only have IEC62368 Ed. 2. So, are there any alternatives…
Part Number: TPS25942A Tool/software: Hi E2E team,
Please help me review the schematic and HW setting for TPS25942A.
Condition:
Vin(normal)=12V
ILimit=1.18A
V(OV)=13.25V
V(UV)=10.85V
In addition, I have the following items that I would…
Part Number: TPS25942A Tool/software: We require a Bidirectional back-back MOSFET for e-fuse application. Part TPS25942A doesnt matches our voltage and current requirements. Our Voltage is 400V and current is 150A. Can you suggest suitable module for…
Part Number: TPS25942A Other Parts Discussed in Thread: TPS2420 , TPS25948 , TPS25947 Tool/software: Hi team, Your products ( TPS25942 and TPS2420 ) are IEC 62368 Ed.3. Are there any plans to change to Ed.4? BR, Kengo.
Part Number: TPS25942A Tool/software: Hi team,
Customer observed that when Vin is removed, PG will pull low. Questions are:
1. how long will PG output low when Vin is removed? what's the min, max, typ value?
2. If Vin drop, what's the max Vin that…
Part Number: TPS25942A Tool/software: Dear team
We are using TPS25942 based active power oring circuit for our custom with power requirementof 12V @5A.
when we powering on our bord, some times our oring IC TPS25942 is getting damaged. As per datasheet…
Part Number: TPS25942A Tool/software: Hi
Is it mandatory to set VPGTH(pin3) as 11V in TPS25942. I am setting this value as 6V for 12V oring application. Please reply