Part Number: TPS25942A Other Parts Discussed in Thread: TPS25940 Hi team,
Could you please suggest a p2p device with TPS25942A. My customers are using TPS25942Aand want a back-up solution.
Part Number: TPS25942A Other Parts Discussed in Thread: TPS61089 , TPS22953 Hi,
I have two different 5v input voltages in my circuit, one of them comes from an adaptor and the other one comes from USB type C connector.
I am thinking about the TPS2594x to…
Part Number: TPS25942A Other Parts Discussed in Thread: TPS2663 , TPS2660 hi
i want to use the TPS25942A to monitor a VIN to the system of 18v(nominal) is there a way to set the Over voltage to monitor ~19v? i dont see it in the tool, and not sure it possible…
Part Number: TPS25942A Other Parts Discussed in Thread: TPS25947 Hi Team,
Would you advise does TPS25942ARVCR has recognition of IEC62368-1 even though
there is a UL 2367 Recognized only in datasheet?
My customer need this information.
Thanks
Best regards…
Part Number: TPS25942A Other Parts Discussed in Thread: BQ25790 , , ASH Hi All,
I'm designing a system with three possible power sources (In priority order).
- 12V DC Input
- 11v - 16v 4S Battery (Main External)
- 11v - 16v 4S Battery (Backup Internal…
Part Number: TPS25942A Other Parts Discussed in Thread: TINA-TI Hi Team.
Currently, a circuit using the TPS25942A has failed within a few days, and I want to find out the cause.(4 out of 4 substrates)
The circuit configuration is the circuit of Figure…
Part Number: TPS25942A Hello expert, I have question regarding TPS25942A. I'd like to know about the source current limitation but datasheet said it is internally limited. Do this mean internal power path can support above highest current which is limited…
Part Number: TPS25942A Hello Expert, I have 2 questions for TPS25942. First, could this device apply voltage up to 20V(Abs max) when input side is opened? I think there is no limitation on output voltage maximum rating due to there isn't such a description…
Part Number: TPS25942A Hello team,
Our customer would like to know why the OUT leakage current in off state is specified for not only sinking but also sourcing.
And they also make sure the conditions for Vout = 18V, V(EN/UVLO) = 0V.
In their understanding…
Part Number: TPS25942A Hi Team,
Here are several questions on reverse OCP.
1. what's the response time, that is, the time between reverse OC is detected to the part take actions?
2. what's the time between the part request to turn off the MOS to the…