Part Number: TPS25947EVM Other Parts Discussed in Thread: TPS25948 The support form only offered TPS25947EVM. Our production design uses TPS259470LRPWR; we are not specifically troubleshooting the EVM. Please route this case to a TPS25947-family eFuse…
Part Number: TPS25947EVM Other Parts Discussed in Thread: TPS25947 Tool/software: Dear Team,
My customer is evaluating the TPS25947EVM, but they have a startup failue and can not continue evaluation.
Please review an attached their settings and measurement…
Part Number: TPS25947EVM Other Parts Discussed in Thread: TPS25947 Hi team,
My Customer uses TPS259474 on their Fan product. When power-off test will have a negative current. but remove C15/C16 from TPS25947EVM.
The negative current will disappear…
Part Number: TPS25947EVM Other Parts Discussed in Thread: BQ25798 , BQ25798EVM Tool/software: We are considering a configuration in which the TPS25947EVM is placed in front of the input of the BQ25798EVM in order to control whether the power input from…
Part Number: TPS25947EVM Other Parts Discussed in Thread: TPS55288 , Hi, Ti teams, we are trying to use TPS25947EVM +TPS55288 (PMIC) to support our Docking USB-C port 20V. we observed the VBUS voltage '
We are attempting to adopt TPS25947EVM +TPS55288…
Part Number: TPS25947EVMTPS25947EVM can not 6A load.
RLIM = 549ohm (initial mounted)
Vin = 12V to 16V
The expected value of the maximum load is 6A .
But, it turned off at 1.1A.
All channel is the same symptom,
I used electrical load,…
Part Number: TPS25947EVM Hi team,
My customer is evaluating TPS25947EVM now and observed The leakage current of Iout depends on Vin.
EN=L, Vin=0V, Vout=7.4V, Iout=-13uA
EN=L, Vin=7.4V, Vout=7.4V, Iout="-79"uA
They have 2 questions.
This characteristic…
Part Number: TPS25947EVM Hello,
I am currently working on the TPS25947EVM evaluation board.
I'm using channel 4 to test the TPS259474L (Latch + Circuit breaker): => Limitation: 0.5A => Input: 15V => Itimer: 18ms => Dv/Dt: no impact on analysis
However…
Part Number: TPS25947EVM Greetings,
We are using a TPS25947EVM and we measured the voltage drop thru the TPS259470 device and back calculated Ron to be 122mohm.
We measured at room temperature, at 1A (0.12V drop), 2A(0.24V), 3A(0.37V) and 4A(0.5V…
Part Number: TPS25947EVM Hi
he customer tested the EVB TPS259474L and encountered several problems. The resistance value calculated by the ILM resistance formula There is a big gap with the actual 3334/2.5A=1.333K Actual 2.12A Shutdown 3334/3A=1.111K…