Part Number: TPS2596 The excel calculator available for TPS2596xx devices has a typo in the drop down box, listing tps259531 instead of TPS259631. Despite the typo, the spreadsheet does not adjust for over voltage lockout above 13.58V. It is not clear…
Part Number: TPS2596 Hello, I am wondering if there are any simulation file available for either TINA or Altium. I am trying to download the PSPICE file here http://www.ti.com/product/TPS2596/toolssoftware , but when I try to import to TINA it gives me…
Part Number: TPS2596 Hi support team,
The ON-Resistance value is written on SLVSET8A. - RON, Electrical Characteristics, Page-7 - Figure-7, Page-10
Only data with IOUT = 0.2A. Does the ON-Resistance depend on VIN and TJ and not on IOUT?
Are the RON values…
Part Number: TPS2596 Other Parts Discussed in Thread: TPS25947 Hi team,
My customer is searching for E-fuse for 15V/2A and -15V/2A use case. For 15V/2A use case, I think TPS2596 is suitable. But for -15V/2A, I not sure if we have any E-fuse than can be…
Part Number: TPS2596 Hi team,
According to the datasheet, table 1, OVC threshold voltage is 5.7V(typ) when 400kOhm resistor is connected. Could you tell how much the threshold voltage will be when 390kOhm +/-5% resistor is connected?
They want to use…
Part Number: TPS2596 Hi team,
Could you let me the definition of tsc?
Is this the time to turn off the FET after the output is shorted? or Is this the time that FLT-pin goes to Low after the output is shorted?
Regards,
Noriyuki Takahahashi
Part Number: TPS2596 Hi team,
I'm considering to use TPS2596 for USB VBUS input protection.
TPS2596 datasheet mentions that input surge capability is HBM:2kV.
Is TVS diode needed for this application in addition to TPS2596?
Regards,
Itoh
Part Number: TPS2596 Other Parts Discussed in Thread: TPS2595 , Hello,
I want to confirm the difference between TPS2595 and TPS2596. TPS2595 and TPS2596 look very similar except for the package and R_ON. Is there any big difference except for the package…
Part Number: TPS25200 Other Parts Discussed in Thread: TPS2596 , TPS2597 Tool/software: Dear technical team
I'm looking for an e-fuse part similar to the TPS25200 but with current monitor capability and better (lower) Iq.
This part is for a battery…
Part Number: TPS2596 I downloaded the TPS259621 file and ran the following sim using values from the spreadsheet. The UVLO should be 4v but I am only getting 1.5 in the sim. I changed the values to force UVLO to 5v, but device still did not turn on. is…