Part Number: TPS2597 Hello,
The datasheet for the TPS2597 only seems to indicate the accuracy of the current monitor gain for currents between 1A & 7.7A. Was the current monitor gain measured for currents less than 1A? If so, could you please provide…
Part Number: TPS2597 Other Parts Discussed in Thread: TPS25948 Hi, I'd like to know if it's permissible to connect a battery charger to the output of the efuse to charge cells connected to the input of the efuse. Other forum comments for similar questions…
Part Number: TPS2597 Hi Team
How to understand the internally limited?
Fro example, what's the value of Vlim limitation? Can you help to clarify the specific value and how is the device limited inernally?
Part Number: TPS2597 Hi team,
The TPS25970LRPWR datasheet contains the following statements: • UL 2367 Certified – File number: E339631 – RILM ≥ 750ohm • IEC 62368-1 CB certified
Questions: What are the advantages of using a UL2367-certified / IEC…
Part Number: TPS2597 Hello team,
We are using the part number TPS25974ARPWR in our existing products, and we are in the process of adding this part to our new products.
Could you provide us with the information and documents.
Headquarters…
Part Number: TPS2597 HI, team,
In the TPS2597x datasheet, ILIM is specified with min/typ/max values. Do these ILIM limits include the tolerance of the external resistor on the ILIM pin (RILIM)?
In addition, when these ILIM limits were defined, what…
Part Number: TPS2597 Hi,
I have an application powered by two rechargeable lithium cells in parallel. Is it possible to connect a separate TPS25974L to each cell, with the Vout from each TPS25974L connected together and then to the charger and to the…
Part Number: TPS2597 Using TPS25974LRPW on output of an isolated flyback power stage with 15V output and 110uF output cap. If I leave DVDT pin floating, what is the minimum output cap of eFuse needed to support steady 1A current through HFET and quickest…
Part Number: TPS2597 Hi sir,
Can TPS25970 enable pin power up before Vin?
https://e2e.ti.com/support/power-management-group/power-management---internal/f/power-management---internal-forum/1613205/tps25982-enable-before-vin?tisearch=e2e-sitesearch&keymatch…
Part Number: TPS2597 Hello,
I have used multiple TPS25974LRPW in a design and one of them sometimes chars itself and fails short. Note that its only in one place where this eFuse fails, the rest are fine. For all other uses of this eFuse, I've used…