Part Number: TPS25981 Tool/software: Hi team,
I see that TPS25981 can be in auto-retry after a fixed delay of removing the circuit-breaker issue. So will it keep auto-retry until the current goes down the setting value?
Part Number: TPS25981 Tool/software: Hi
I am investing an issue on our prototype board where the eFuse is failing sometimes short circuit (well measuring 7ohms on DVM in both directions) the UVLO is not operating and the device just passed input to output…
Part Number: TPS25981 Tool/software: Dear Team,
I have the following queries regarding the TPS259814A IC:
(1) Ground Splitting:
As per the EVM, the ground is split into power ground and IC ground and connected together through 0 Ohm 0603 Resistor. However…
Part Number: TPS25981 Other Parts Discussed in Thread: TPS25982 Tool/software: Hello experts,
I am planning to use TPS259814ARPWR on my board to to protect against high current. The LOAD current is about 12A and I have to set the protection when the current…
Part Number: TPS25981 Other Parts Discussed in Thread: TPS25980 , TPS25982 Tool/software: I have a question. I would like to use this IC in a 12V output voltage line with a 7.5A current limit. Would this IC be a suitable choice? Even if the load tries…
Part Number: TPS25981 Tool/software: Hello,
What is the current rating of PG and nFLT for TPS259814ARPWR and where can I find that information in the datasheet.
Thanks.
Part Number: TPS25981 Tool/software: Hi team,
TPS25981 is 2mm*2mm package, the Rja is 49.7.
But for TPS259260, it is 3mm*3mm, the Rja is 45.9.
TPS259260 has larger package so the thermal resistance should be lower, correct? But the fact is they are…