Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS25981
Hi Team,
Can you please add Iout = 8A and Iout = 10A to this plot from the datasheet (or share an excel sheet with test data):
Assuming Ta = 25C, what would ~Rdson be at the following operating points...
3.3V / 1A
3.3V / 8A
3.3V…
Part Number: TPS25981
Hi,
The datasheet for the TPS25981 states that the ILIM ranges from 1.5A to 11A, is it possible to set a current lower than 1.5A with ILIM?
Thanks,
Astro
Part Number: TPS25981 Hi,
I have a question regarding the minimum voltage on the EN pin of the TPS25981.
As far as I can see from the datasheet, the the minimum voltage on the EN pin is 0.5V. Is it a problem to connect GND to EN/OVLOpin?
Thanks,
Astr…
Part Number: TPS25981 Other Parts Discussed in Thread: TPS25940-Q1 , TPS4811-Q1 Hi! I am a member of a Formula SAE team and we are trying to design a custom Smart Power Distribution Fuse board. We found the TPS259814ARPWR and it checks all of the design…
Part Number: TPS25981 Hi,
Can you please explain what the recommended over voltage and under voltage set point is for 3.3V and 5V application? We are having an internal discussion and I like to understand what are the recommended % of over voltage and…
Hi Arush,
Is there any update information to our question? We want to know if there is a risk on TPS2421 in using resistors instead of CT capacitors.
We will replace TPS2421 with TPS2597 or TPS25981 for further design.