Part Number: TPS25982 Hi,
I am using part TPS259822ONRGER in a design where the input voltage is nominally 15V, whereas the device I assembled has Vovlo as 3.7V
I SHOULD HAVE used a part such as TPS25982 7 ONRGER, but only realized my mistake when testing…
Part Number: TPS25982 Hi,
We are going to use this eFuse in power side in our design with load condition. I need to know the fuse will work or not.
If the part will not work with load condition means, please recommend alternate part for our condition…
Part Number: TPS25982 Hi,
I'm testing the TPS259827O and I've configured the autoretry pins as following:
- RETRY_DLY open
- NRETRY open
As the datasheet specifies, I'm expecting the device to retry 4 times with minimum delay during an over current…
Part Number: TPS25982 Hi
i need a out put capacitor calculation for this part.or can you please give the WEBENCH link,because i need to verify the differnt current level.
Part Number: TPS25982 Hi team,
We have few question about this device design.
In datasheet figure Figure 46. Input Line Transient and Output Short-Circuit Response shows two type start-up "current limited" and "dVdt limited".
Q1. Does…
Part Number: TPS25982 Dear Sir/Madam,
I'd like to perform the failure analysis of my schematic, which contains the TI eFUSE of TPS259823ONRGE.
But I can't find the Pin FMA document for this component from the website.
Would you please help to confirm…
Part Number: TPS259824OEVM Other Parts Discussed in Thread: TPS25982 Hello all,
Does TI have an IC that performs the functions of TPS25982 and LM4700 in one package? If not, are there any recommendations to connect the above IC together?
Best regards
…
Part Number: TPS25982 Hello Sir:
Please refer our load current profile as below figure.
Our input voltage is 16.8V and max continue current is around 4.5A.
Please help to check our schematic.
If there has any setting cannot meet our load profile or…