Part Number: TPS25982 Tool/software: Hello, I have two questions about the current limiter:
1. When running the current limiter to 2.5A load, but not full short, my expectation was that the current limiter would directly drop the output voltage and…
Part Number: TPS25982 Tool/software: Hello,
I am using TPS25982 IC the below is the circuit diagram
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/pastedimage1727269782827v6.jpeg
While testing output short…
Part Number: TPS25982 Other Parts Discussed in Thread: TPS25983 , Tool/software: Hello everyone,
We are working with the Fab house and encountered an issue with the soldermask and pastemask of the footprint, which were built based on the recommended…
Part Number: TPS25982 Tool/software: Hi,
When the EN is disabled, we want to know the leakage current through the output pin to GND. Input voltage to the device is 15V. This leakage current does not seem to be specified in the datasheet.
Thanks, I…
Part Number: TPS25982 Other Parts Discussed in Thread: TPS25983 Hi
Is there any efuse or hot swap available for this line that can be replaced?
for removable batteries
Do hot plug on the input
Part Number: TPS25982 Tool/software: Hi Sir,
For Datasheet figure.51, the auto-retry priority is the thermal shutdown or the current limit?
For Datasheet figure.53, it means the TPS25987x output power in start-up time that must be under 80W and…
Part Number: TPS25982 HI, the question is not related to the reflow phase but on the PCB layout.
In the component datasheet you have this figure as a layout example
There is no thermal relief on the pad. Do you recommend NOT to use the thermal reliefs…
Part Number: TPS25982 Dear Team,
We are designing TPS25982 and have some questions as below. Could you share your comments with us?
1. what is PD on R_ILIM? What resistor size we need to design with? (0402 or 0603)
2. In design calculation tool…
Part Number: TPS25982 Hi,
I am using part TPS259822ONRGER in a design where the input voltage is nominally 15V, whereas the device I assembled has Vovlo as 3.7V
I SHOULD HAVE used a part such as TPS25982 7 ONRGER, but only realized my mistake when…