Part Number: TPS259827LEVM Hi team,
My customer is evaluating TPS259827L with our EVM (TPS259827LEVM). They configured the EVM for 15A current limitation and apply a 24V input power supply. The problem is the system cannot start up if they connect a…
Part Number: TPS259827LEVM Dear Expert ,
Good day!
Our customer use the TPS259827 with 3A Electromagnet , the device can not start up . Here is the shcematic
I had told him to test the Vin /Vout signal wave with load or without load , here is…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: TPS25982 The data sheet states “UL 2367 Recognition (pending)” and “IEC62368 CB Certification (pending)”. Do you have any updated status of the certifications?
Hi Mohamed Sidiq,
The device should turn OFF to a Circuit Breaker Fault when the RETRY_DLY pin is shorted to GND.
Can you re-confirm if the RETRY_DLY is properly connected to GND
Can you share the following waveform captures when the device…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: TPS25982 Hi team,
My first time designing a board and I have been trying to calculate the values based on the calculation tool. With the TPS259827L, the Over Voltage Protection is only at 16…
Part Number: TPS259827LEVM We were testing the TPS259827LEVM eval kit with an electronic load at 24V. The current limit was set to 5A. The output voltage was the same at free load, but when we set the load to 2A the output voltage dropped to around 20V…