Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS25983 Other Parts Discussed in Thread: TPS25982 Tool/software: Dear Team,
We are planning to use TPS25983 eFuse for the medical device we are designing. I could see UL certification is pending for this. Could you please say when will it…
Arush Gupta said: Are you seeing this even after adding the above mentioned FETs?
Not to the same extent - I am still seeing ~400mV of backdrive at 85C and ~200mV at 25C.
Part Number: TPS25983 Tool/software: Hi,
I am working on a design using the TPS25983 and I would love to simulate the behavior of the chip, but we are looking at the TSP259830O variant with circuit breaker functionality and the website only has a spice…
Part Number: TPS25983 Tool/software: I'm qualifying ICs and as a part of preliminary risk assessment I'm looking for any information about fabrication process. TI releases PCNs, and sometimes there is a such information. But in case of TPS259830ONRGE…
Part Number: TPS25983 Tool/software: Hello,
we want to limit the current flow, but with different limits depending on the direction. To achieve this, application note SLVA948 suggests to connect two efuses back-to-back:
Regarding this setup with the…
Hi Christian,
It looks like i missed this thread.
I also don't see any issue with this but will still recommend evaluating this on the board.
Best Regards, Arush
Part Number: TPS25983 HI ARUSH
thank you for your reply
I would like to know the maximum and minimum values of retry time.
How much capacitor value do I need to set to set to 3 seconds?
thank you.
Part Number: TPS25983 Other Parts Discussed in Thread: TPS25947 Hello Team, We are planning to use the IC TPS25983 for over current protection. The output of the device will be connected to a number of LEDs . The total output current will be 3.5A. The IN…
Part Number: TPS25983 Other Parts Discussed in Thread: TPS1211-Q1 , LM74900-Q1 Title: Technical Inquiry about TPS25983 eFuse - Maximum Short Circuit Handling Capability
Hello Texas Instruments community,
I am currently working on a project that involves…
Part Number: TPS25983
Hi,
I Have a problem with the OVLO calculation. UVLO is used as enable from MCU.
Here, it is noted to start with R1=1MOhm. However, if you use the Excel calculator tool (V1.40), it ends up being in the kOhm values (R1 = 10.8k…