Part Number: TPS25984 Other Parts Discussed in Thread: TPS25990 , Dear Sir/Madam of TI support engineer,
We are currently prototyping a new OEM product using your eFUSE (TPS259840RZJR). We want to start the VOUT output several tens of milliseconds after…
Part Number: TPS25984 Hello Sir,
We use eFuse IC (TPS259840RZJR) for our motor driving protection.
Our circuit works in our lab (our schematics & PCB board works); When it is running in the field, we found that TPS259840RZJR give both Pin 5 (FLT)…
Part Number: TPS25984-CALC
Hi,
I was looking at using the TPS25985-CAL however no matter the input the RIREF doesn't change (stuck at 40k) so I think the calculator doesn't work properly. Is this correct?
SLVRBL0 — TPS25985 Design Calculator
Part Number: TPS25984 Tool/software: According to "7.3 Recommended Operating Conditions" the voltage on the PG pin can be 0-5V. On p52 of the datasheet there is a "CAUTION" stating that PG must be between 2.5-5V. Can you please clarify the voltage range…
Part Number: TPS25984 Tool/software: Greetings - I am looking for transient thermal response curves for this device. Is that available? If not, can you tell me the size of the die? I can estimate the thermal response if I know the die size. Thanks!
Part Number: TPS25984 Hi,
Please provide the design calculator for the part. In datasheet application information section, it is written that a spreadsheet design tool 'TPS25984x Design Calculator' is available on request.
Thanks,
Akhil
Part Number: TPS25984
• Regarding this part number "TPS259840RZJR"; We checked your website and we did not find the required chemical data for this part, so we still need the chemical composition data (Total part Weight (g)-Homogeneous Material Location…
Part Number: TPS25984B Other Parts Discussed in Thread: TPS25984 Tool/software: Hi Team,
Hope everyone is doing well.
I'd like to know the difference between the TPS25984 and TPS25984B.
I've observed that the peak current can be increased to 70A…
Part Number: TPS25985 Other Parts Discussed in Thread: TPS25984 Hello TI Support,
We are using two TPS259850 devices in parallel, configured according to the Primary/Secondary architecture:
Primary MODE pin: floating
Secondary MODE pin: connected…
Part Number: TPS1686 Other Parts Discussed in Thread: TPS25984 , TPS1685 , LM5067 Tool/software: Hi TIer
My customer want to choose two power switch or efuse. Could you help me check and give some suggestion? Thank you very much.
-5V (maximum -6V…