Part Number: TPS25990 Tool/software: HI TI
https://dev.ti.com/gallery/view/PowerSwitches/TPS25990x/ver/2.0.0/
I used the TPS25990 online GUI to perform the installation, but I encountered an error during the installation process. Could you please…
Part Number: TPS25990 Tool/software: Hi Team
below is my customer SCH for MP5998.
could you help me point out which part should they modify to use TPS25990 to replace MP5998.
MP5998_591P2.pdf
BRs
Brian
Part Number: TPS25990 Tool/software: Dear Sir:
Refer to the datasheet, read MFR_MODEL (9Ah): Read the part number of the chip. Block read ASCII values – “TPS25990” = 0x54, 0x50, 0x53, 0x32, 0x35, 0x39, 0x39, 0x30.
But my IC reads 0x54, 0x50, 0x53…
Part Number: TPS25990 Other Parts Discussed in Thread: USB2ANY Tool/software: We have production stop due to incompatible / changed TPS25990 device.
We have been using the device for a while, but on the latest board batch we read a different "MFR_MODEL…
Part Number: TPS25990 Tool/software: TPS25990 EN/UVLO pin setting
I tried setting the EN/UVLO pin to 1.4v, but PG pin always low and Vout=0.6V
How to set it up to improve? Vin=6.0V Thanks
Part Number: TPS25990 Hello,
My customer requested TI's review of the circuit for the TPS25990ARQPR.
Please review the customer's circuit below to ensure there are no problems.
TPS25990ARQPR_SCH_20251114.pdf
Thank you.
Part Number: TPS25990
Tool/software:
Hi Expert,
In switch applications, the ambient temperature inside the chassis may be as high as 60°C. In this case, what is the recommended maximum RMS current? Is it reasonable to use RθJA = 19.9°C/W for evaluation…
Part Number: TPS25990 Other Parts Discussed in Thread: TPS25985 , Tool/software: Hi team,
May I know what's the short current threshold when it have one TPS25990 parallel with one TPS25985?
Does it count together? 158.8A + 290A = 448.8A ?
How it…
Part Number: TPS25990 HI TI,
I found that adjusting the RIOMN setting in the WEBGUI does not change the checksum. Does this mean that the configuration on the web only affects the calculation of the displayed values in the WEBGUI?
BR,
DELUN