Part Number: TPS2640EVM Hi team,
Pls help confirm the test report result is okay or NOT. customer reply some result not meet spec.
TPS2640EVM test report.pdf
Part Number: TPS2640EVM Hi team,
Overcurrent testing is typically performed using direct current (DC).
However, will the results be different when applied to fans?
Because the current waveform will be pulsed rather than pure DC.
Customer use TPS2640EVM…
Part Number: TPS2640
I am working on one project. In that, I am using TPS26400RHFR as protection ic.
I refer same circuitry for my project with TPS2640EVM Schematic
but my circuit is not working.
input = 24VDC
output get zero voltage…
Part Number: TPS2640EVM The TPS2640EVM shows an additional 24.3KOhm resistor in series with the Cdvdt, which is not shown or explained in the datasheet.
Why was this resistor introduced and is it mandatory to populate this resistor?
Best Regards,…
Part Number: TPS2640EVM Hi,
Good Day. Is there available CAD Model for TPS2640EVM? Customer is need to create a housing for the EVM. Please advise. Thank you very much.
Best Regards,
Ray Vincent
Hi devaraju,
TPS2640EVM: Evaluation Module for TPS2640
4.4.3 Current Limit and Fault Responses Test section in EVM user guide
I have followed EVM user guide instructions, please do follow the same instructions & test it in same format.
thanks…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS2663 , TPS2640EVM , TIDA-03031 Dear Sir, Madam,
in our application we want to develop a surge protection with TPS26600 and performance criterium A.
In App note SLVA833D the performance criterion…
Part Number: TPS2640 Hi,
I've got two questions regarding TPS2640 eFUSE. I noticed some discrepancies between the documentation for the IC and the evaluation board, hence the questions.
1. In the diagram of the evaluation board, a TVS diode (D8) is…