Part Number: TPS26600-02EVM Tool/software: Hello, I just did tests at 10V with TPS26600 eval board with the RHF side of the board. I removed J13, J14, J11, J10. I installed J8 and J9. J12 is set to position 1-2 so that 5.36K resistor is used. Testing…
Part Number: TPS26600-02EVM case cs2268231
T1/VIN1 = 5V 100mA J1 - Jumper ON J2 - Jumper ON J3 - Jumper OFF J4 - Jumper ON 1-2 J5 - Jumper 7-8 connecting R12 200mA. J6 - Jumper OFF J7 - Jumper OFF
TP4 SHDNb1: Attached to system Digital Output to control level…
Part Number: TPS26600-02EVM I used this ic TPS26600RHFR for protection. I set the current limit of 1.67A startup load current is zero ,only 1870uF capacitor charges during starting.
After capacitor is fully charged I gave load of 1A ,so it is generating…
Part Number: TPS26600-02EVM Dear TI,
Can your review the below eFuse circuit
Nominal Voltage 12VDC
Load Current Max 1.5A
Under Voltage: 6V DC
Over Voltage: 20V DC
Revers Polarity and 2.3A of current Limit
Part Number: TPS26600-02EVM Hello, I have the EVM configured as follows:
I have a bench top power supply set to 51 V and 3 A, with 440 uF in aluminum electrolytic and ~ 6.6 uF of MLCC capacitance connected just upstream of the EVM V_IN. Downstream I have…
Part Number: TPS26600-02EVM Hi,
Could I get hold of the design files for the TPS26600-02EVM, preferably Altium Designer? I'm interested in the best way to do the copper pours for RTN/thermal management.
Thanks
Part Number: TPS26600-02EVM Hi,
I have a 48V 3phase motor controller in production that is having thermal issues (Bus Capacitors Poping).
My team has isolated the root cause of this failure to 2 circuits, both of these circuits are 48V, protected with…
Part Number: TPS26600-02EVM Other Parts Discussed in Thread: TPS2662 Hi Team,
We're using the TPS26600-02EVM and set the device to 'Latch off' mode using J4 (pins 1-2 shorted) , J5 set to 7-8 position.
We're using 12V / 300mA and when…
Hello Vashist,
I am also getting similar results with simulations.
It will be accurate to check on TPS26600-02EVM which is available on ti.com.
Thanks
Amrit
Part Number: TPS26600-02EVM Hello
I was trying to change the OVP threshold on the TPS26600 EMV and replaced the R8 and R3 with calculated values, but I noticed that the OVP was still 32.4V and not 31.6V as I wanted it to be. When I measured the resistance…