Part Number: TPS26600-02EVM Hi,
Could I get hold of the design files for the TPS26600-02EVM, preferably Altium Designer? I'm interested in the best way to do the copper pours for RTN/thermal management.
Thanks
Part Number: TPS26600-02EVM Hi,
I have a 48V 3phase motor controller in production that is having thermal issues (Bus Capacitors Poping).
My team has isolated the root cause of this failure to 2 circuits, both of these circuits are 48V, protected with…
Part Number: TPS26600-02EVM Other Parts Discussed in Thread: TPS2662 Hi Team,
We're using the TPS26600-02EVM and set the device to 'Latch off' mode using J4 (pins 1-2 shorted) , J5 set to 7-8 position.
We're using 12V / 300mA and when…
Part Number: TPS26600-02EVM Hi Sir,
My customer using TPS266600 and PCB is back,
When TP68=5V , VBUS no any o/p
R129 1K change to 0 ohm, sometimes VBUS has 5V o/p, sometimes no o/p.
R129 1K remove , VBUS has 5V o/p
Pls comment if below circuit is correct?…
Part Number: TPS26600-02EVM Hello
I was trying to change the OVP threshold on the TPS26600 EMV and replaced the R8 and R3 with calculated values, but I noticed that the OVP was still 32.4V and not 31.6V as I wanted it to be. When I measured the resistance…
Part Number: TPS16630-32EVM Other Parts Discussed in Thread: TPS26600-02EVM Tool/software: Hi,
Q1 The TPS26600-02EVM documentation states "Load current monitor output with 1.5 V / A" and uses R(IMON) of 20 [kΩ]. Is it correct that the IMON output range…
Part Number: TPS26600-02EVM Hello,
We use TPS26600 with 200ma input limit and still face inrush currents around 3A. We tried removing D1, C35, C75 to no avail. We also tried increasing C77 value to 1uF, 2uF to no avail.
Can you please guide us regarding…
Part Number: TPS26600-02EVM Hi team,
Customer use our calculation tool to calculate IMON resistor.
But the calculation result is different from the datasheet.
If l(LIM) is 1A, so R(IMON) is 33.3k, right?
I suggest him follow the datasheet first.
Many…