Part Number: TPS2662 Hello, I am currently designing the power supply input for an industrial module that needs to meet the following specifications:
19.2-28.8V (24V nominal) external power input, reverse input protected
Protect load up to 60VDC…
Part Number: TPS2662 Hi team,
Could you please clarify two points regarding the specifications of the TPS26621DRCR?
1. Is there a specified operating humidity range for the TPS26621DRCR? I have reviewed the datasheet, but I could not find this information…
Part Number: TPS2662 I am trying to determine the exact input-to-output propagation delay time for the internal power path MOSFETs during an overvoltage lockout (OVLO) event.
Specifically, I am looking for the time duration from the exact moment the…
Part Number: TPS2662 Hi,
We need to use the eFuse for the overcurrent protection and the min. limit current is 150mA,
because of the issues with the usage environment, the external temperature is more than 135 Celsius degree,
we use TPS26625 for…
Part Number: TPS2662 For the PO - 37H179683, the MPN showing the TI backlog report is TPS26621DRCT . But, we need the MPN to changed to TPS26621DRCR . Also, please provide the price for the MPN - TPS26621DRCR. We need the changes to be done immediatley…
Part Number: TPS2662 Hi,
I'm using the TPS26625 as a switch, enabled via the SHDN pin. Others designs tend to use the GND as a reference for this pin, but i'd like to use the integrated reverse polarity protection provided via the RTN reference.
1…
Part Number: TPS2662 Hello,
I am evaluating the TPS26621 eFuse and have run into what appears to be a design contradiction involving the UVLO/OVP resistor ladder, the pin voltage limits, and the recommended operating conditions. I have described the…
Part Number: TPS2662 Hello Team,
We have connected RTN to GND for thermal performance enhancement as our system doesnot require the Reverse Input polarity protection feature.
Can you please let us know if RTN-GND connection affects any other feature…