Part Number: TPS2662 Tool/software: Hello
Using the TPS26621DRCx to protect an LED Illumination circuit for factory automation devices (multiple types, some with and some without microcontrollers).
If there is not a microcontroller in the circuit, the…
Part Number: TPS2662 Other Parts Discussed in Thread: BQ25628E
Tool/software:
Hello,
I have been trying to implement the TPS2662 e-fuse IC on a board and am encountering some issues. For context, the circuit that this e-fuse is a part of is intended…
Part Number: TPS2662 Other Parts Discussed in Thread: TPS2660 Tool/software: Hi team,
Is there any simple HV(48V) Hotswap solution? output current 1A
TPS2662 seems not to support the hot-swap function. Thanks
Part Number: TPS2662 Tool/software: Hello,
I am testing the TPS2662 eFuse capabilities in order to replace it with a high side pMOS switch. My duty is to protect this high side switch from overcurrent condition (which is pretty impossible with a simple…
Hello Patrick,
Yes, there can be leakage path from OUT to GND.
Different voltage for different batch could be result of both charging current and total impedance.
Thanks
Amrit
Part Number: TPS2662 Tool/software: Hi,
I have a quastion about the "Shutdown pin" (pin 4).
1. what is the value of the inside voltage "Avdd" that the pullup resistor pulled ?
2. See below the schematic and the connection as I use…
Part Number: TPS2662 Tool/software: Refer to link below, it looks like I have the same issue. From the link it's look like TI has contact directed to customer and solved it, right? Do you have any suggestion if we should power the U2 with VB0 instead…
Part Number: TPS2662 Tool/software: Hello,
The TPS26622 calculator doesnt consider the case where UVLO pin is connected to RTN to disable it. R2 and R3 cant be set to 0ohm or removed.
Besides that I would like to understand what is the voltage rating…
Part Number: TPS2662 Tool/software: Hello,
We are using TPS26625DRCT IC in one of our designs, I have attached its schematic circuit image and PCB file in which the required IC is having designators U28 and U29.Can you please review the attached layout…