Part Number: TPS2663 Other Parts Discussed in Thread: TPS1663
Tool/software:
Hi,
I'm trying to simulate this component TPS26630RGER in LTSpice
But I keep getting error saying "too few nodes "
how can I fix this as this simulation is critical…
Part Number: TPS2663 Tool/software: Hello.
I have a problem with the slew rate of the output voltage. Sometimes the slew rate is correct - around 100 ms, and sometimes it is only around 500 us. I attached some waveforms of situations described:
Conditions…
Part Number: TPS2663 Tool/software: Hello,
I have a design that is using the TPS26630 E-Fuse and is powered by a power supply whose output is rated above 250VA.
According to UL 2367, this E-Fuse is only supposed to be powered by a power supply whose…
Part Number: TPS2663 Tool/software: I had a design using TPS2663.
Cannot start the circuit when using a switching power supply, no problem when using a bench top power supply.
What can be the cause?
Regards
CS
Part Number: TPS2663 Tool/software: Hello Rakesh,
I have the same questions, could you also send me the distribution data? Thank you.
Kind regards,
Thomas
Part Number: TPS2663-166EVM Other Parts Discussed in Thread: TPS2663 Tool/software: I am planning to use eFuse part number TPS26631PWPR in our new project, Input voltage range is 10.8 V to 52.8V, and 1.5A, Can you please provide me the reference schematic…
Part Number: TPS2663 Other Parts Discussed in Thread: TPS2660 Tool/software: Dear,
I need to use your TPS2663 eFuse in our application to protect a DC/DC converter with DC power supply in the range 4.5-30V. We need a configuration in order to pass the…
Part Number: TPS2663 Tool/software: Hi, in my application, Im trying to connect a TPS2663x to a motor controller board which has 10mF of capacitor on board with 200W max. Using the calculator, I noticed that the device will go into thermal regulation…