Part Number: TPS26630-33EVM Other Parts Discussed in Thread: TPS2663-166EVM Hi there,
are the schematic/layout files for the boards TPS2663-166EVM and TPS26630-33EVM available?
Kind regards,
Laura
Hello Ramesha,
Thanks for choosing TPS2663 part in your design.
Reference schematic you can find in below EVM user guide
www.ti.com/.../TPS26630-33EVM
Thanks
Amrit
Part Number: TPS2663 Hi expert,
I noticed that TPS26633 will automatically go into the voltage clamp situation when OVP is trigged. And the duration for the voltage clamp is 162ms.
My question is if the fault is removed in the duration, could TPS2663…
Part Number: TPS26630-33EVM Other Parts Discussed in Thread: LM5069
Hi,
I did some tests on TPS26630-33EVM board. I'm using DC load and battery. EVM is not latching-off like overcurrent fault while undervoltage stage. When I disconnect the load, voltage…
Part Number: TPS26630-33EVM Other Parts Discussed in Thread: TPS2663 , TPS2662 , TPS2660 Hello Expert,
Our customer want to test IEC610000-4-5 Level 3 w/ this EVM and it is their spec.
Vin is both adaptor 12V or PoE 48V.
Could you give us what's the additional…
Part Number: TPS25940 TPS26630-33EVM
Hi,
We're developing an automotive product using some design reference from TI. I'd like to know if our schematic is reliable and are there anything else details could be applied to?
1. we also have to pass…
Part Number: TPS26630-33EVM Other Parts Discussed in Thread: TPS2663 Hi Team,
Customer downloaded the calculation table of TPS26630 fromTi.com as attachment.
The calculation table is protected, could you provide me password to unlock calculation file.
…
Part Number: TPS26630-33EVM Other Parts Discussed in Thread: TPS2663 The evaluation board is rated for surge protection up to 500V (IEC610000-4-5 Level 1). I was hoping to modify it to handle up to 4kV (IEC610000-4-5 Level 4).
I have an operating voltage…
Part Number: TPS26630-33EVM Hello,
I am wondering why in the TPS26630-33EVM two of the No Connect (NC) PINs are being used. PIN#19 with VOUT and PIN#24 with VIN1?
The other NC PINs are all connected to GND.