Part Number: TPS272C45 Datasheet not specifying minimum overcurrent limit threshold at overload condition.
How to ensure, under normal load condition, overload not triggered ?
For instance: Rlim=10k, Iload=2A --> max. DS value is 2.42A, min. value…
Part Number: TPS272C45 Other Parts Discussed in Thread: TPS274160 Hello,
I am designing to the new TPS272C45A as a replacement for the very out-of-stock TPS274160BRLH. In the TPS274160BRLH datasheet ( https://www.ti.com/lit/ds/symlink/tps274160.pdf…
Part Number: TPS272C45 Hi team,
Simulation on TPS272C45C shows the output voltage is clamped at -2V from ground, without any external TVS/diode connected. If there is no internal clamp in TPS272C45C, I would expect the voltage should be much more negative…
Part Number: TPS272C45 Other Parts Discussed in Thread: TPS274160 Hello,
I am using the TPS272C45 as follows:
VS = 24V
Logic Vdd = 3.3V, inputs driven by a micro
In the Absolute Maximum Ratings, some of the upper limits are specified as VS:
…
Part Number: TPS272C45 Other Parts Discussed in Thread: TPS27SA08 , Hi,
I had some time for further testing the samples of the PTPS272C45ARHFR.
I didn´t find an information about quiescent current for single supply, both channels disabled and diagnostics…
Part Number: TPS272C45 Hi,
My customer wanted to know if it is possible to tie together the two channels to act as a single switch and get a higher current value.
Regards,
Vanessa
Part Number: TPS272C45 Hello,
In figure 10-1 of the datasheet, there is an optional reverse polarity protection circuit, in which certain connections must go to module GND instead of device GND.
First of all, I interpret "module" to be the local…
Part Number: TPS272C45 Other Parts Discussed in Thread: TPS2HB50-Q1 , TPS4H160-Q1 Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "VNQ7050AJTR" ?
https://www.st.com/resource/en/datasheet…