Part Number: TPS274160 Hi expert,
My customers are not planning use the fault and ST pin for TPS274160, how should they config these pins, can they just simply float them?
Also, If plan not using FAULT pin, would this affect the device‘s normal use…
Part Number: TPS274160 Other Parts Discussed in Thread: TPS274C65CP , Tool/software: we are using the TPS274160ARLHR IC as load switch with 4 channels with max of 2A each. as per the datasheet it can deliver up to 4A on each port, is that correct understanding…
Part Number: TPS274160 Tool/software: Hello TI experts,
I'm using the TPS274160BRLHR to design four PLC-Type digital outputs 24V, and I have a question about protecting these outputs.
According to TI recommendations, we've included a Cout of 22 nF…
Part Number: TPS274160 Tool/software: Hi team,
I had a problem with conducted emissions exceeding the standard, And now I ’ m looking for the source of emission,.
I checked TPS274160A data sheet and didn't find some information about CE (conducted…
Part Number: TPS274160 Tool/software: Hello TI-Team,
the ranges of the pulldown resistors of the enable inputs are given in the datasheet for an input voltage of 5V.
It would be necessary for me to know these resistor ranges over the whole possible…
Part Number: TPS274160 Tool/software: Hi E2E,
Our customer is using TPS274160ARLHR to design a product. Some SCHs are as follows:
The problem we encountered was that the voltage of +500V could pass through the ESD surge test; the voltage -500V…
Part Number: TPS274160 Tool/software: Hello,
In the data sheet it says
"For better protection from a hard short-to-GND condition (when the ENx pins are enabled, a short to GND occurs suddenly), the device implements a fast-trip protection to turn…
Part Number: TPS274160 Hello TI team,
I would like to ask you if it is possible to have the functional safety manual for TPS274160 available or I should apply in a specific form to get it. Thank you in advance.
Best Regards,
E.P
Part Number: TPS274160 Tool/software: Hello TI team,
concerning the recommended GND network to protect the TPS274160 I have.the following questions.
1) GND network to protect against turning off of inductive loads If the outputs of the TPS274160 are…