Part Number: TPS274160 Hello,
I'm using the TPS274160B at my design.
I'm not using the current sense function, only the current limit function, so I put the DIAG_EN in high state, and the SEH and SEL at low state (open).
My question is, if there…
Part Number: TPS274160 I have Systems where i only need to use half the drivers at a time (half the drivers move the machine 1 direction, half move the other). If im only using half the drivers at a time, can i get 2.5A on 2x of the 4x drivers while the…
Part Number: TPS274160 Other Parts Discussed in Thread: TPS272C45 Team,
We’re using this in a design application where we will be enable 1 channel at a time and not all 4 channels together.
Can a single channel support 35W output ? (Not all 4 channels…
Part Number: TPS274160
Hello,
At the TPS274160 datasheet, it is stated that the Td,rise, is maximum 150uSec.
But dV/dton, which is one of Td,rise parts, is 0.1V/uSec, which means that with 24V supply, the rise time from 10% to 90% can be 240uSec.
In…
Part Number: TPS274160 I'm getting ready to use the TPS274160EVM that I received today and in looking through the documentation, the circuitry used to set SEL and SEH on the TPS274160EVM doesn't seem quite right. A screenshot taken from the PDF…
Part Number: TPS274160
Hello,
I've downloaded the TPS274160B pspice model for Orcad Pspice model.
I used it at Orcad Pspice 16.6, and it worked fine.
I tried to use it at Orcad Pspice 17.4 (meaning that I added the library at the simulation profile…
Part Number: TPS274160 Hi Team,
I have a few questions on the TPS274160.
1. If we just use 2 out of the 4 channels of this device, can we do 2A per channel? The datasheet states that 1.35A/channel is possible with all channels on.
2. Current limit is…
Part Number: TPS274160 Hello,
I've been using the TPS274160EVM in order to examine the TPS274160 behavior.
1) When I shorted output number 4, and looked at the CS diagnostics pin, I expected to see 4V, according to the TPS274160 datasheet, but instead…
Part Number: TPS274160 Hi, Good day. Our customer has a project where they would need 4 outputs limited each to 1A. They want to use the TPS274160 and they want to know if the current limiting resistor needs to be set to 1A or 4A? Thanks in advance Regards…