Part Number: TPS274160EVM Hi Sir,
My customer received the TPS274160EVM, but they found the EVM used the TPS274160B, but the schematics of the EVM user guide drawled the TPS274160A.
Could you please share the correct schematics with us. Thanks!
Part Number: TPS274160EVM Hello,
At the TPS274160B datasheet it is stated that the outputs are tolerant to voltage surge of 1kV over 1.2/50uSec.
At the TPS274160B EVM there are optional TVS diodes at the outputs.
The suggested TVS diodes are…
Part Number: TPS274160 I'm getting ready to use the TPS274160EVM that I received today and in looking through the documentation, the circuitry used to set SEL and SEH on the TPS274160EVM doesn't seem quite right. A screenshot taken from the PDF of the…
Part Number: TPS274160
In Section 8.3.7.4, Reverse-Current Protection , the datasheet states:
"The reverse current protection diode in the GND network forward voltage should be less than 0.6 V under any circumstances."
However, in Table 9-1 of the…
Part Number: TPS274160 Hi Dear,
As shown in the figure,referring to the TPS274160EVM evaluation board, the CS pin is connected to a pull-up resistor. What is the function of the pull-up resistor? However, in the datasheet of TPS274160, the typical application…
Part Number: TPS274160
Hello everyone,
I am currently in the process of designing a PCB with a TPS274160A (the version without the current sense capability) and I have questions regarding the GND network and and the selection of an external TVS diode…
Part Number: TPS274160 Hello,
I've been using the TPS274160EVM in order to examine the TPS274160 behavior.
1) When I shorted output number 4, and looked at the CS diagnostics pin, I expected to see 4V, according to the TPS274160 datasheet, but instead…