Part Number: TPS2819 Other Parts Discussed in Thread: TPS2829 Hi team,
My customer is trying to use TPS2819 with the external 13.7V supply from LDO.
VDD and VCC are tied as well as Figure 20 in the datasheet because the customer doesn’t want to use the…
Part Number: TPS2819-EP Hi Aaron Grgurich,
Sorry for the late reply. There was a document about ESD of TPS2819MDBVREP. www.ti.com/.../sgzk021.pdf
There is the following description. Referenced Method: EIA/JESD22-A114 EIA/JESD22-A115 JESD22-C101
From the above…
Part Number: TPS2819-EP Hi Team
Could you tell us ESD(HBM/CDM) spec of the following items?
1:TPS2819MDBVREP
2:UC1842AMDREP
3:UCC2818MDREP
Best regards'
Minami
Part Number: TPS2819 Other Parts Discussed in Thread: TPS2829 Hello Team,
the TPS2819 and TPS2829 share the same datasheet and the difference is about the internal regulator.
pin 1 is NC on the TPS2829 while it is Vdd on TPS2819.
If we would use the …
Part Number: TPS2819 Hi Team,
Just want to confirm, in the datasheet (Dissipation Rating Table), the power rating at Ta=80°C is 227mW, but using the derating factor 3.5mW/°C, I always got 245mW. For Ta=70°C, I got the same 280mW. Is there anything that…
Part Number: TPS2819 I am using TPS2819 to drive MOSFET IRF540.
Mosfet is driving Proportional Solenoid.
I am facing issue with few of my drivers burning after working for more than 3-4 months.
PWM from miceocontroller is 5V @ 250HZ.
I am attaching my…
Part Number: TPS2819 Hello,
Hope you are doing well!
I tried to simulate the mosfet driver TPS2819 using NOR gate(SN74HC27D) but found that TPS2819 is not giving desired output.
Please verify below simulation and let me guide if any error are there.
…
Part Number: TPS2819-EP Other Parts Discussed in Thread: TPS2819 , Hi,
I am using TPS2819 Driver to drive a MOSFET. I would like to calculate the Turn-ON time of the MOSFET. To calculate the same, I need the Driver resistance. Can you share the same?
…
Other Parts Discussed in Thread: TPS2819 , TPS2818 , TPS2816 , TPS2817 , TL5001 , TPS2819-EP , TPS2818-EP Hello,
I was going through the datasheet of TPS28XX - EP. There was one Contradictory statement.
Statement in page 2 mentions -
"The TPS2816 and TPS2817…