Part Number: TPS2832 Other Parts Discussed in Thread: UCC27282 , TPS28225 , LMG1210 Hi,
I would like to use the TPS2832 to drive a half-bridge in a SRC/LLC type converter that is controlled by a single input clock of 50% duty cycle. To ensure proper…
Part Number: TPS2832 Hi,
The Theta J-A & Theta J-C parameters of TPS2832 is not available in the datasheet. Could you share the same?
Regards,
Veerasamy
Hi Aleksandr,
Thanks for your interest in our driver, my name is Mamadou Diallo from the High Power Drivers team.
The Absolute Maximum Ratings section specifies the stress levels that, if exceeded, may cause permanent damage to the device. However…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…
Siyu,
I think the toggle flip-flop in the block diagram on page one of the spec should have let you know that the max you will get with this device is 50% duty.
Go to page 43 and 44 of the attached and select a more suitable part.
Peter,
i am enclosing the Power Management Guide for 2011. The section you will be interested in starts on page 43 and actual devices listed on page 46, With the minimum information you have given me I would expect that you will want something like…
Hi,
I've attached the 2013 User's Guide for power products. Starting on page 53 you will find a selection of PWM controllers. many of these teh frequency can be varied according to external criteria.
As an example if you use a UC3842 it is a simple…
Gary,
Most any of our power controllers with dual output capability will provide the control. See attached document starting at page 50 with the dual output controllers on page 53 and 54 and choose what features you want.
Regards,
John