Part Number: TPS2HB16-Q1 Other Parts Discussed in Thread: TPS2HB35-Q1 , TPS1HB50-Q1 , TPS1HB35-Q1 Hello,
We are considering TPS2HB16-Q1 for our design to switch the load current (heater load ) and plan to set external over current limit to 4.5 A, In the…
Part Number: TPS2HB16-Q1 Hello!
What are the upper and lower limits of the Rsns resistance that can be set for TPS2HB16?
If it is less than 1kΩ, what is the limit resistance value that can flow Isns correctly?
If it is larger than 1kΩ, what is…
Part Number: TPS2HB16-Q1 Hi,
We are using TPS2HB16-Q1 in our design to control the heater load in industrial application.
Can you please clarify below point ,
If there is a over current or short circuit fault in one of channel (say channel 1) then as…
Part Number: TPS2HB16-Q1 Hello Team,
For TPS2HB16-Q1 - whatis value for VOL,off (parameter mentioned in datasheet section 9.3.3.1.2 ) ?
Is the the same as VOL in EC table at datasheet beginning (2Vmin, 3Vtyp, 4V max)?
Part Number: TPS2HB16-Q1 Other Parts Discussed in Thread: TPS2HB35-Q1 , TPS2HB50-Q1 TPS2HB35 TPS2HB16 and TPS2HB50 whether there is a difference in current measurement accuracy?
Part Number: TPS2HB16-Q1 Hello,
We are using the HSS TPS2HB16-Q1 to control hydraulic proportional solenoid valves with PWM frequency of 200 Hz.
The valve comsumption is around 1.2~4 Amps/12volts (the worst case is the 4 Amps valves).
We are also using…
Part Number: TPS2HB16-Q1 Hello,
my customer is currently foreseeing the TPS2HB16-Q1 in a BMS design and they would like to know if there is a limit in for this device with respect to the frequency of operation of their application (between 20 - 25 KHz…
Part Number: TPS2HB16-Q1 Hi team,
Could you tell me how much current limit ratio min and max is for TPS2HB16 A -Q1?
I am interested in current limit ICL min and max value. I found that ICL = KCL / RILIM shown in equation (1). To decide ICLmin and ICLmax…
Part Number: TPS2HB16-Q1 I am using TPS2HB16-Q1. I am using both channels. When I am giving 3.3V to EN1 then I get Vout1 12V, but when I am giving EN1=0V then I am getting Vout1= 4V instead of 0V. It should be off. But in channel2 is working fine. I am…