Part Number: TPS3103 Other Parts Discussed in Thread: TPS3899 , TPS3808E Hello,
I have a customer who is currently using the TPS3103. We are looking for any cost down opportunities to present to them. I just wanted to check with you if there are newer…
Part Number: TPS3103 Dear team,
I am looking for dual channels reset IC like our TPS3103 but need open drain output and programmable delay time function?
Could you recommend reset IC solution to us?
Thanks,
Ben
Part Number: TPS3103 I'm hoping you can help - we've seen some strange behaviour from the TPS3103 chip. Although this state is rare we have measured, with a DVM, that the output voltage is measuring at 0.97V and holding the device in a reset state even…
Part Number: TPS3103 Hi Team,
My customer notice TPS31xx family can work in a temperature range of -40℃ to 125℃. But in PACKING INFORMATION section, all the TPS31xx family's op temp is -40℃ to 85℃.
They want to know which one they should take reference…
Hi Team,
This is customer request, can you please advise:
"
- TPS3103E15DBVR
- TPS51206DSQR
- TPS82130SIL
I need IBIS models of 3 parts. Do you have a chance to share?
"
Thanks in advance
Furkan Sefiloglu
Part Number: TPS3103 I am looking for a circuit that is useful for testing the effect that different doses of radiation have on the performance of the TPS3103 chip. The circuit should be able to test the relevant performance before radiation, during …
Question/Problem:
The PFI pin is stuck at 0.64 volts no matter what the input voltage is.
Answer: The voltage on PFI should be the 1.8V divided down by the resistor divider and track the changes in the 1.8V line. If it is stuck at 0.64 the device…
Part Number: TPS3801 Other Parts Discussed in Thread: TPS3103 Dear SIR: (continue before question ,because didn't reply)
Thank for your reply.
But,May I double confirming :
(1) according to your reply:
Is that meaning as below ?:
For VDD pin…