Saif,
We don't typically provide the ATE Lot Data and we can only guarantee that Vsense will be between the MIN and MAX values listed in the Electrical Characteristics table found in the datasheet. I know that TPS3306 is around 2% voltage sense accuracy…
Hello all,
I have a tricky trouble whit TPS3306-18. I use this component whit a tri state buffer on pin WDI so i can use internal retrigger. Usually when pin is tri stated i see train of short pulse spaced by about 800 mS. This should be the internal…
Other Parts Discussed in Thread: TPS3306 Hi,
I need to know how can I do to start TPS33'6 when I switch on my board and microcontroller doesn't run correctly so I haven't first toggle on WDI and WDT TPS3306 doesn't start.
I need that it start alone…
Other Parts Discussed in Thread: TPS3306 I have a customer that is using TPS3306 and they belive noise is coupling into the WDI input.
This is a weakly driven pin that toggles and looks for transitions. How is this pin sampled during transition? Is…
We are using the TPS3306-18 with Vdd = 3.3V and Sense1 = 5V, Sense2 = 1.8V. At ~20C power up we are seeing the part apparently latch up with the part driving reset and the oscillator not running. We can tell this by putting a FET probe on the power pins…
Hi team,
page 5 of the datasheet ( http://focus.ti.com/docs/prod/folders/print/tps3306-33.html ) tells us:
By connecting two external resistors, it is possible to supervise any voltages above 1.25 V. The sum of both resistors should be about 1 M W…