Part Number: TPS3307 Tool/software: Hi TI Team,
Our customer requested the ESD please help to provide it.
Material name : TPS3307-33DGNR
Best regards,
Takako Fujiya/TED
Part Number: TMS320F28335 Other Parts Discussed in Thread: TPS3307-18-Q1 , The reset pin of TPS3307-18-Q1 is of push-pull type. When it is connected to the XRS pin of TMS320F28335 (which is supposed to be of open-drain type), what kind of abnormalities…
Part Number: TPS3307 Hi team,
My customer wants to know if the device will get damaged when >VDD+0.3V is applied to SENSE3. From the related thread, I understood that SENSE3 should not exceed VDD+0.3V, which is shown in the recommended operating range…
Part Number: TPS3307 Hi experts
Customer is using TPS3307-33 with 3.3V VDD, but they are wondering that if SENSE3 can be tolerant with higher voltage than VDD+0.3V(like 5V). Since I notice that <VDD+0.3V is our recommendation but it's below 7V.
Is…
Part Number: TPS3307-EP Hi, everyone
I have a question about TPS3307-33MDGNREP.
What signal is PowerPAD(thermal pad) connected to internally?
Also, is there a problem connecting the PowerPAD to GND?
Part Number: TPS3307 Hi
I got a question from my customer about TPS3307-18.
This device is not written ESD ratings in datasheet.
Does this device define ESD rating?
Or could I refer to ESD protection value of TPS3307-18M?
Best regards…
Part Number: TPS3307-EP Other Parts Discussed in Thread: TPS3704 , TPS3704-Q1 , TPS3307 Hi,
Is there a version of the TPS3307-18MDREP voltage supervisor part with and open drain output reset pin, instead of push-pull? If not, is there a similar pin…