Part Number: TPS3430 Tool/software: Hi team,
If WDI is input while WDO is outputting low, Trst becomes longer than the set value (200 ms)
Will Trst be extended if WDI is input while WDO is low?
Part Number: TPS3430-Q1 Other Parts Discussed in Thread: TPS3430 Tool/software: Hello
we are using this TPS3430 as windows watchdog with CYT2B74 MCU(5V),
but whenever we connect the debugger/ winades tool at the JTAG_RESET connector for debugging…
Other Parts Discussed in Thread: TPS3430 Tool/software: Hi all,
Im testing a prototype PCB we have developed and we are using the TPS3430 as part of the circuitry. We send a pulse to the WDI input inside of a 1-10ms window to keep the output enable…
Part Number: TPS3430-Q1 Other Parts Discussed in Thread: TPS3430 Tool/software: Hi expert,
Is there any concerning points when TPS3430-Q1 use in that once Vdd down 1.6V
Is there any other voltage conditions that need to be met after falling below…
Part Number: TPS3430 the datasheet states "WDO delay time can be set to any value between 700 μs (CCRST = 100 pF) and 3.2 seconds (CCRST = 1 μF)"
I need at least 5s for reset. Is it really not possible to use a 2.2uF cap in CCRST?
thanks
Part Number: TPS3430-Q1 Other Parts Discussed in Thread: TPS36-Q1 Tool/software: Hello Expert,
Could you please tell me when TPS3430-Q1 start count down of WD first pulse if pin is configure as WD=Enable at power-up?
Timing Diagram as X duration…
Part Number: TPS3430-Q1 Tool/software: Hi Team,
In the datasheet, '8.2.2.1 Design Requirements - Design 2' mentions the maximum device current consumption. The max current is 200uA according to the design requirement, but in the design result the current…
Part Number: TPS3430-Q1 Tool/software: Hi team,
My customer has 2 questions regarding TPS3430-Q1's pin connection, can you help advise?
1. Are the SET0 and SET1 pins open-drain outputs? Do they need to have pull-up resistors when connected to a high…
Part Number: TPS3430-Q1 Tool/software: Hello Expert,
Could you please tell me pin status of WDO(pin8) during power is off?(e.g. Hi-z short-to-GND, weak pull-down, etc)
Our customer want to know this information for estimating abnormal condition…