Part Number: TPS3431-Q1 Customer reported that TPS3431-Q1 has no package info listed on datasheet (as below image)
Would you check if this can be shared ? Thanks.
Part Number: TPS3431-Q1 Hi I would like to understand the operation when WDI is default pulled up and no falling edge pulse happens. On my board, I also have WDO pulled high and I don't see it going low. Can you please provide guidance on if this is the…
Part Number: TPS3431-Q1 Tool/software: Hello Application team
May I know what's the EN pin pull high resistor value range since we would like to evaluate the GPIO connection.
thank you
Part Number: TPS3431-Q1 Tool/software: Hi Sir,
would like to clarify if the C CWD can use 10uF or 22uF to set the longer CWD time or not? because the C_CWD capacitor is test between 100pF and 1uF in the datasheet.
may we use 10uF and 22uF for longer…
Part Number: TPS3431-Q1 Tool/software: Hi Sir,
The datasheet specify the Typ. "minimum WDI pulse duration" is 50ns.
We would like to know the Min. and Max. pulse duration requirement for WDI.
Thanks,
Ocean
Part Number: TPS3431-Q1 Other Parts Discussed in Thread: TPS3431 , TPS3430-Q1 , Hi Team,
There is a good new that we could DIN TI product!
The customer wants to find the watchdog with the same specifications as TPS3431 but conforms to the Automotive…
Part Number: TPS3431-Q1 Other Parts Discussed in Thread: TPS3436-Q1 , TPS3435-Q1 , , TPS3431 TPS3431SDRBR We would like to know if there are any Watchdog timers/ any other device available, which will not be reset(as attached below from the datasheet…
Part Number: TPS3431-Q1 Hi team,
i would like to know,
when EN is pulled low, the watchdog timer is stopped or reset to 0?
when SET1 is pulled low, the watchdog timer is stopped or reset to 0?
when SET1 is pulled low, WDO will change to high…