Part Number: TPS3613-01 Tool/software: The table on page 2 of the datasheet implies the positive RESET output (pin 7) should be the opposite of the /RESET output all the time. The rest of datasheet implies these pins are always push-pull outputs.
However…
Part Number: TPS3613-01 It is unclear of the expected behavior of both the RESET and ~RESET outputs of the TPS3613-01 when the VDD pin has no power (0V) and the VBAT pin has 3.6V.
Looking at the function table, it appears RESET could be high, but its…
Part Number: TPS3613-01 Hi Team,
We have three questions.
---------
[Q1]
We would like to use backup-battery switchover function with Electric double layer capacitor.
I think that VDD, VBAT, SENSE, VOUT pins are the following circuit.
Could you please…
Part Number: TPS3613-01 Other Parts Discussed in Thread: TPS3619 Hello team,
The datasheet mentions that the VBAT is connected to VOUT via 15 Ohm switch.
Is this PMOS or NMOS?
If so, is the leakage lower than 100nA when VDD=3.3V and VOUT =3.0V?
I found…
Part Number: TPS3613-01 Hello team,
my customer is using TI TPS3613-01 device for 1.8V main power(VCC_1V8_B) and 1.8V battery power(BAT_1.8V) SRAM backup application.
They have a issue with battery backup. Normal operation with main power(VCC_1V8_B…
Part Number: TPS3613-01
Hello,
We currently use the TPS3613-01 to manage battery backup for the SRAM (SRAM part number: IS62WV51216BLL-55TLI) on our PCB. We are trying to determine the battery life of the coincell battery if our product is powered off…
Part Number: TPS3613-01 Hi Team,
Attached my customer issue with TPS3613, please help.
Thanks,
Shlomi
TPS3613 - Strange behavior - MAJOR issue - Production is on HOLD.docx
Part Number: TPS3613-01 Dear Specialists,
My customer is considering TPS3613-01 and has a question.
I would be grateful if you could advise.
---
Could you please recommend how we should terminate the unused pins(SENSE, MR and RESET) for unused?
---
…
Part Number: TPS3613-01 Other Parts Discussed in Thread: TPS3831 , TPS3839 , TPS3890 Dear Sir
I could not find ESD rating data like ESD-HBM/CDM in this datasheet.
Customer requested us to show ESD rating of TSP3613-01DGSG4.
Would you share this ESD data…