Part Number: TPS37-Q1 Hi team,
In order to avoid voltage drop at SBD in red circle below, I would like to connect SNESE pin directly to VBAT terminal.
TVS diode is placed as below.
I concern reverse battery condition and ISO 7637-2 pulse1(-100V), pulse3a…
Part Number: TPS37-Q1 Other Parts Discussed in Thread: TPS37 Hi team,
I have a question about TPS37_38-Q1 Functional Safety pin FMEA description below.
"For fixed voltage threshold option where the applied voltage to SENSE1 is less than 2.7V...."…
Part Number: TPS37-Q1
Hi team,
Is there any requirement in order of SENSE and VDD voltage rampup/down?
From Absolute Max rating perspective, both pin has 70V rating, so there should be no issue even if bias is applied to SENSE pin without VDD.
Is there…
Part Number: TPS37-Q1 Good morning,
is there a LTSpice working model for TPS37-Q1?
When I run the model available on the website, I obtain the following error:
Thank you very much for your support.
Marco
Part Number: TPS37-Q1 Hello team,
Please tell me the minimum guarantee values of tSD and tCTR when CCTR1/MR = CCTR2/MR = Open. I want TPS37-Q1 to output RESET for a certain period of time. I would like to know if there is enough period for tSD(min) and tCTR…
Part Number: TPS37-Q1 Hi team,
Could you please advise the definition of Vhys parameter in the datasheet EC section?
If I select VIT=800mV and 2% hysteresis version, is it "+/-1.5% of VIT(800mV)=0.012V" or "+/-1.5% of VIT*2%=0.00024V"?…
Part Number: TPS37-Q1 Hi team,
Could you please advise if reset release time delay (tctr) is added after I release Manual reset pin Low to High-Z?
I understand sense delay is ignored when Manual reset is driven Low from Hi-Z, and I would like to confirm…
Part Number: TPS37-Q1 Other Parts Discussed in Thread: TPS37B-Q1 Hi Team,
Could you please check the below selection table between TPS37B-Q1 and TPS37F-Q1?
Is it same function device? if so, which one should be used for production?
Best regards
Joey…
Part Number: TPS37-Q1 Hello,
The datasheet has conflicting information on the TPS37H output logic. In table 8-2 it shows ch1 = OV OD H, ch2 = UV OD L. While in the device comparison section (page 3) the H suffix is shown to be ch1 = OV PP L, ch2 = UV OD…