Part Number: TPS3700 Other Parts Discussed in Thread: TLV809 , TPS3840 , TPS3510 , TPS3710 Hello team,
I would need a voltage supervisor to verify that the input stage with 12V..250V input rail is generating an output voltage of at least 7V (generally between…
Part Number: TPS3700TPS3700 is for monitoring of a window of power (over voltage and under voltage). do you have a chip do two under voltages monitoring such as one for 7 voltage and another for 6 voltage with 9 v power supply?
Very appreciate your support…
Part Number: TPS3700 What should be the values for R1, R2 & R3 for the following, while using TPS3700 window comparator,
Over Voltage Limit is = >5.6 V
Under Voltage Limit is <= 4.4V
Can anybody give me a solution.
Part Number: TPS3700
Hi team, Customer measured the TPS3700 Tphl is 32us. On the TPS3700 datasheet, it only has nom value 18us. Is 32us the expected timing?
BR, SHH
Part Number: TPS3700 Hi Team,
TI p/n TPS3700DDC has number of packaging options: TPS3700DDCR, TPS3700DDCT and TPS3700DDCR2
For some reason those pats have different device marking:
TPS3700DDCR and TPS3700DDCT - with marking PXVQ
TPS3700DDCR2- with marking…
Part Number: TPS3700 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hello,
I'm doing a temperature simulation with the TPS3700 in LTspice (since I don't know how to do in TINA), and I'm seeing strange behaviour…
Part Number: TPS3700 Hello Team,
Does TPS3700 have internal input protection diodes to VCC and GND?
How much current is allowed to go through these diodes (if placed)?
Thanks and Best Regards,
Hans
Part Number: TPS3700
Hi Team, My customer is designning the TPS3700. Could you explain for how to get the Vhys min and max values' conditions? And how to calculate the Vit+-Vit-=12V?
It seems not match the Vit+ and Vit- min and max table.
Thansk…
Part Number: TPS3700 Other Parts Discussed in Thread: TPS3806 , Customer are using with TPS3700DDCR to monitor the main battery of the car.
How we can add hysteresis on the input voltage?
Hysteresis of 3v
or Do we have any other comparator from this series…