Part Number: TPS3701 The datasheet of TPS3701 does not specify the drift in threshold voltage because of ageing. What is the drift in threshold voltage because of ageing? Is it already included in the specified tolerance in datasheet?
Part Number: TPS3701 Other Parts Discussed in Thread: LM4040 Hello,
I need to protect the VDD input of a TPS3701 from voltage surges of 60 -0/+3 Vdc for 100 ms and then a reduced voltage of 40 -0/+2 Vdc for 1 second.
Attached is the circuit I designed…
Part Number: TPS3701 Other Parts Discussed in Thread: TPS3700 日本語で通じそうなので日本語で質問します。
過日TPS3701の出力にマイナス電圧は掛けられない、との回答を得ましたが。
まだ方法を探っています。
マイナス電圧はデータシートで0.3V迄掛けられるとなっています。この時の流出電流はどこまで許されますか?
当コンパレーターでVOUTA/BがLowの時、High Impedance (例えば1MΩ)でマイナス電位…
Part Number: TPS3701 since system environment is bad, the power supply would susceptible to voltage transient and noisy, it would be causing the fault operation of the OUTA and OUTB during motor is in operating. Customer would like to enhance the noise…
Part Number: TPS3701 Hi,
The voltage of the INA and INB inputs are limited to voltages between -.3 to +7 volts per spec. Is it correct to assume that there are two diodes connected to each input for static protection (clamping the input between approximately…
Part Number: TPS3701 Hi Team,
I am using TPS3701.
1. For monitoring only undervoltage (only INA) of a rail which is different from VDD, how to calculate R1 and R2? There is no detail specified in datasheet for this configuration.
2. Any alternate…
Hi Michiaki,
Is it possible for you to draw out the schematic? I am having a hard time picturing what you are describing. Are you suggesting using two TPS3701 devices where one of them monitors the 16V rail while the other one monitors the output of…