Part Number: TPS3702 Hi,
The calculator excel sheet which can be downloaded, does not list TPS3702AX12.
Do we have a smiilar calculator available for this IC?
Thanks and regards
Part Number: TPS3702 Hello,
Let me confirm about below.
* According to datasheet DC spec, when user will use TPS3702C with ""SET" pin = High".threshold is set to "+/-4%".
In addition, accuracy of threshold is +/-0.9% at over…
Hi Abhishek,
Unfortunately there are no currently released similar higher accuracy TPS3702-Q1 type devices. The last option for UV would be to go with a device like TPS3703E4080DSERQ1 and use high accuracy resistors to set the adjustable threshold. For…
Part Number: TPS3702 The specifications in Table 6.6 of the data sheet show nominal times only. Is there a specification for the maximum startup delay, TSD?
Part Number: TPS3702-Q1 Hello Team,
according to the data sheet the max current into Vsense-Pin is specified with 1.5uA at Vsense = 5V. This is valid for TPS3702CX50, correct?
Question: Will the Vsense current be proportional to Vsense voltage or will is…
Part Number: TPS3702 Dear Support Team,
We are planning to use TPS3702AX12 IC in our product.
Is this part available commercially? Can you please share its price, MOQ and availability information with me?
Thanking you in advance.
Part Number: TLV3702-Q1
Hello Team,
according to the data sheet the max current into Vsense-Pin is specified with 1.5uA at Vsense = 5V. This is valid for TPS3702CX50, correct?
Question: Will the Vsense current be proportional to Vsense voltage or will…
Part Number: TPS3702-Q1 Hi team,
What’s the orderable part number of tps3702-Q1 if it’s used to monitor 3.3V power rail with ±5% accuracy?
From blow table, it seems tps3702AX33 is the right choice.
However, tps3702cx33 is recommended…
Part Number: TPS3702 Other Parts Discussed in Thread: TPS3700 , TPS3701 Deas TI-Support team,
was looking for window voltage monitor (separate UV, OV outputs in OD configuration) to supervise a processor core voltage. Processor datasheet specifies a recommended…