Part Number: TPS3703-Q1 Other Parts Discussed in Thread: TPS3703 , TPS3702 , TPS3704 There are 4 graphs in datasheet regarding sense glitch immunity (figure 7-11 to 7-14). Furthermore there are typical values in table in section 7.6. Unfortunately the values…
Part Number: TPS3703-Q1 Hi Expert,
I have some questions about TPS3703-Q1 as below. Could you please help to clear?
Is LATCH mode only available when CT pin is connected to GND? For CT pin connected to VCC or cap, it is not available, right?
Is internal…
Part Number: TPS3703-Q1 Hi,
To anlayse the logic compatibility, could you please help with the VIL,VOH,VIH data of the supervisor TPS3703A7120DSERQ1.
Thanks & Reagrds,
Reshma
Part Number: TPS3703-Q1 Hello,
I have some questions as down below:
1. What timing is starting to count 450us to determine the reset time delay? When VDD> UVLO or VDD>= VDD(min)?
2. Does ICT re-charge the CT pin when RESET goes back to deasserted…
Part Number: TPS3703-Q1 Other Parts Discussed in Thread: TPS3703 Hi Team,
How do I confirm the external resistors design that is correct?
For example:
Conditions: Monitor voltage target: 2.4V, IC's sense pin: 1.2V
Combinations:
1. (R1: 1Mohm , R2: 1…
Part Number: TPS3703-Q1 Other Parts Discussed in Thread: TPS3703 Hello everybody,
i use a TPS3703A4180 to monitor the power supply TPS73118. So in my design VDD of TPS3703 and VSense is the same.
Due to the Datasheet this is not a problem. But I do net…
Part Number: TPS3703-Q1 Hi team,
My customer has a question about section 9.1.4 of the datasheet. The last paragraph talks about checking the effect of Rsense on the accuracy of the resistor divider.
If the equations 4 and 5 are used as is to calculate…
Part Number: TPS3703-Q1 We have a concern that noise may trigger the MR when the device is configured in LATCH mode - CT pulled to GND via 10kohms (MR/n with only 25nsec of glitch immunity + 100K weak pull-up).
Please confirm that it is acceptable to…
Part Number: TPS3703-Q1 Hi team,
My customer is considering using TPS3703-Q1 for monitoring 5V power rail. They would like to know if the monitoring voltage continue to exceed to above the maximum rating of 6V, IC itself will be damaged, will the reset…